Technical FAQs

Ask a Question

MET 148-2 8-Temperature Sensor Module Installation Sheet, Instruction Bulletin (ANSI),

The MET 148-2 module can connect eight temperature sensors (RTDs) of the same type:

• Pt100, Ni100, or Ni120 type RTDs, according to parameter setting
• Three-wire temperature sensors

The temperature measurement provides for thermal overload and temperature monitoring.

See attachment:

Was this helpful?
What can we do to improve the information ?