Technical FAQs

Ask a Question

Can Remote Control be enabled from the advanced UMI of the Sepam Series 20, 40 and 80 Relay?

For the Sepam Series 20 and 40 relay
"remote control" can be activated by navigating through the front face of the Sepam relay.
Go to general settings -> Modules -> Modbus. Scroll down until the remote control screen appears


Note: "SBO" means Select Before Operate
For the Sepam Series 80 relay

"remote control" cannot be activated by navigating through the front face.
In order to activate this setting, connect to the relay using the SFT2841 Software kit with the CCA783 cord.
"Remote Settings" is located under the "General Characteristics" tab of SFT2841.



 
Was this helpful?
What can we do to improve the information ?