Technical FAQs

Ask a Question

How many operations can the circuit breaker do

The vacuum circuit breaker (Evolis) used in MCset is capable of 10,000 operations on full load (not full fault current interruption)
The SF6 circuit breaker (LF) used in MCset is capable of 10,000 operations on full load (not full fault current interruption)

For more information on the circuit breakers used in MCset please click here
Was this helpful?
What can we do to improve the information ?