Technical FAQs

Ask a Question

What is an arc tunnel and why do we need it

An arc tunnel is fitted on the top of the cubicle over the top arc vent flaps. It is used when the substation ceiling height is less than 4 metres. The tunnel is used to vent hot arc gasses out of the substation into a safe area.
Was this helpful?
What can we do to improve the information ?