Technical FAQs

Ask a Question

What is the IP rating of GenieEvo

The standard IP rating of GenieEvo is IP3X.

Alternative IP ratings are available: -

  • IP31
  • IP4X
  • IP41
Was this helpful?
What can we do to improve the information ?