Technical FAQs

Ask a Question

Are the KNB16CM* tap-off units (Canalis Evolution) available not equipped with the C60N modular circuit-breaker, for on-site mounting?

No, because it is difficult to install a circuit-breaker in the tap-off unit without special tools, which are only available in the installation factory.
Was this helpful?
What can we do to improve the information ?