Technical FAQs

Ask a Question

How many stop bits do the Momentum Modbus ports manage?

Momentum processors and the 172JNN21032 communication adaptor only manage one stop bit. Any attempt to change the number of stop bits will be ignored. All the other port parameters can be changed.
Was this helpful?
What can we do to improve the information ?