Technical FAQs

Ask a Question

What parts are required to enable a K1 or K2 cam switch to be mounted in a distribution board?

For mounting a K1 or K2 in a distribution board (panel) there is a 'cam switch installation kit', part number KZ91H

The KZ91H kit comprises the following parts;
  • Mounting plate
  • 45 x 45 mm front plate without legend
  • Black handle (KZ27H) length 35mm
  • 2 fixing screws

Was this helpful?
What can we do to improve the information ?