Technical FAQs

Ask a Question

What material is used for the enclosures of the VCF*GE or VCFXG** type Vario switch disconnectors?

The enclosure bases and covers of enclosed VARIO switch-disconnectors, part numbers VCF*GE or VCFXG**, are made of Makrolon 6385. The fire resistance of this material is: 960 Deg C according to standard IEC 695-1, V0 according to standard UL94, I3F1 according to NF F16-101.
Was this helpful?
What can we do to improve the information ?