Technical FAQs

Ask a Question

When mounting a KCF1PZ handle on an enclosure door, should the gasket be fitted inside or outside the door to ensure a degree of protection of IP65?

The gasket must be fitted on the outside of the door, between the faceplate of the handle and the door.
Was this helpful?
What can we do to improve the information ?