Technical FAQs

Ask a Question

What is the resistance of the contact for the XY2TP type safety mats?

The resistance of the contact of XY2TPx safety mats is:
  • less than or equal to 5 ohms at closed state
  • equal to 10 Mohms at open state
The rated operating characteristics of the contact are 30 VDC for 100 mA.
Was this helpful?
What can we do to improve the information ?