Technical FAQs

Ask a Question

Is there a single pressure switch which can be used to detect the difference between two different pressure sources?

This type of pressure switch is included in the SQUARE D offer as follows:



The full part number will be 9012 plus the number in the table, e.g. 9012GGW1. In the UK, please contact Industry Technical Support on 0870 608 8608 for a quotation
Was this helpful?
What can we do to improve the information ?