Technical FAQs

Ask a Question

What is the minimum bending radius of the cables type ABE9XCA**** used with the ABE9 splitter boxes?

The diameter of the cable type ABE9XCA**** used with the ABE9 splitter boxes is 10.6 mm (+- 5%).

The minimum bending radius (radius of curvature) is 5 x diameter for a fixed installation and 10 x diameter for a moving (flexing the cable) installation.


Was this helpful?
What can we do to improve the information ?