Technical FAQs

Ask a Question

With an RM6, can I use DIN fuses instead of FUSARC fuses?

No, only FUSARC CF or SIBA fuses are compatible with RM6 cubicles. FUSARC fuses are specified in DIN 43625.
Was this helpful?
What can we do to improve the information ?