Technical FAQs

Ask a Question

What is the life of an RM6 cubicle mechanism and what servicing is required?

The life of the RM6 cubicle is 30 years. The mechanism is guaranteed to 1000 operations. Under normal operating conditions no maintenance is required during this period. Beyond that, regular checks should be made.
Was this helpful?
What can we do to improve the information ?