Technical FAQs

Ask a Question

What is the internal arcing withstand for an RM6 cubicle?

The internal arcing test, although not obligatory, is provided for in the appendix to standard IEC 60298. It is based on an agreement between the manufacturer and the operator. RM6 cubicles have been successfully tested with a 20 kA internal arc for a period of 1 second.
Was this helpful?
What can we do to improve the information ?