Technical FAQs

Ask a Question

Can I connect another Sepam 2000 on CTs used to ensure earth leakage protection (Sepam 2000)?

Yes, you can connect more than one Sepam 2000 (or Sepam 1000/1000+) to a single set of CTs while still ensuring earth leakage protection. Caution: This does not apply to the Sepam 100LD. This Sepam is self-powered and distorts the current supplied by the CTs.
Was this helpful?
What can we do to improve the information ?