Technical FAQs

Ask a Question

What is the maximum length of the cable connecting a CSP sensor and a Sepam 2000?

The CSP sensor is connected to the Sepam 2000 by means of a coaxial cable with a maximum length of 5.5 m (CCA 601).
Was this helpful?
What can we do to improve the information ?