Technical FAQs

Ask a Question

What information is contained in the cartridge of the Sepam series 80?

The cartridge of the Sepam series 80 contains the following information: The system and application software (protection functions, settings and parameters). The customised command and control functions (matrix, equation editor, customised logic, etc.). The customised operating language. This information is saved if a power failure occurs on the Sepam. Caution: Never remove the cartridge when the Sepam is powered up.
Was this helpful?
What can we do to improve the information ?