Technical FAQs

Ask a Question

To what does the cycle time of the Sepam series 80 correspond?

The cycle time is the time taken by the Sepam series 80 to carry out all rapid functions. Within a fixed cycle time of 14 ms, the following functions are carried out: Self-tests. Protection functions. Update of logic inputs. Control logic. Equation editor. Update of logic outputs. Some of the slow functions (measurements).
Was this helpful?
What can we do to improve the information ?