Technical FAQs

Ask a Question

What types of temperature probes can be connected to the Sepam 1000+?

Sepam 1000+ can measure up to 8 temperatures for improved overload protection of motors and transformers.

Three types of temperature probes can be connected to the 8 inputs of the optional module of the Sepam 1000+:
  • Pt100
  • Ni100
  • Ni 120
Was this helpful?
What can we do to improve the information ?