Technical FAQs

Ask a Question

What are the advantages of the new MET148-2 temperature module for Sepam 1000+?

The new MET148-2 module replaces the MET148.
It allows up to 8 temperature probes to be connected, for measurement and protection purposes. Available since May 2002, it offers the following features:
  • Replacement for the MET148 already available for Sepam series 20, 40 and 80
  • Improved safety and reliability for temperature measurements
  • Use of two modules with Sepam series 40 and 80 (NB: only one module for Sepam series 20):
    • to use this facility, set the address for each module (with the power off)
    • Only the old module that was used is compatible with Sepam series 20 and 40.
Was this helpful?
What can we do to improve the information ?