Technical FAQs

Ask a Question

Can I connect 2 sets of current sensors on the Sepam 80? (one set with LPCT sensors and the other with In/5A or In/1A sensors)

Yes, two sets of current sensors can be connected to a Sepam series 80.
Both traditional current sensors (In/5A or In/1A) and LPCT sensors can be connected.
Only Sepam series 80 using transformer earth leakage protection (Sepam T87, M88 and G88) do not allow the use of LPCT sensors.
Was this helpful?
What can we do to improve the information ?