Technical FAQs

Ask a Question

Can I directly connect the voltage inputs of the Sepam series 80 on a 415V LV system?

No, the Sepam must not be connected directly to the network. The continuous thermal withstand of the voltage inputs of the Sepam series 80 is 240 VAC. The Sepam parameter setting tool (SFT2841) does not allow such a voltage to be entered.
Was this helpful?
What can we do to improve the information ?