Technical FAQs

Ask a Question

Do I need to protect by password access to the remote setting of a Sepam 1000+?

No, a password is not required for remote changes to the protection settings of the Sepam 1000+ via the Modbus communication bus. Remote setting can be disabled by means of a parameter setting in each Sepam 1000+. Access control for this function should be programmed in the SCADA. Remote setting of the Sepam 2000 is based on the same principle.
Was this helpful?
What can we do to improve the information ?