Technical FAQs

Ask a Question

Can forced ventilation be provided on a TRIHAL dry type transformer?

If there is a temporary overload, forced ventilation can be installed to avoid overheating of the windings.

For ratings above 630 kVA, TRIHAL  transformers used in the UK have provision for the future fitting of cooling fans as standard, as such forced ventilation can be fitted on to an existing installed transformer to obtain a temporary 40% increase in power.

TRIHAL transformers for use in the UK can also be supplied with the fans fitted at the time of manufacture to provide the 40% increase in power

For ratings below 630kVA it is required that the need for forced cooling in the future is advised at the time of order so that the transformer can be designed to accommodate the fans

If cooling fans are to be fitted to a TRIHAL transformer,  the following points must be taken into account: due to the increase in power rating
     The cross-sections of the cables or busbar trunking

     The rating of the transformer protection circuit breaker.
     The sizing of the air intake and outlet apertures in the transformer room for ventilation purposes

     The service life of the fans, which is much shorter than that of the transformer (3.5 years as against 30 years).
Was this helpful?
What can we do to improve the information ?