Technical FAQs

Ask a Question

Can I use a standard auxiliary contact block on LC1D or LC1K contactors specific to "Capacitors"? Can I have the auxiliary contact block only?

The contact blocks for LC1D or LC1K contactors specifically designed for capacitor switching are a precoupling block with resistive wire connections which are specific to each type of  capacitor switching contactor. This is to ensure that the auxiliary contacts close before the main contacts on the contactor. As a result, these  contact blocks are not supplied separately from the contactor.
Was this helpful?
What can we do to improve the information ?