Technical FAQs

Ask a Question

What is the life of the "teach" key on the XX930 range ultrasonic sensors?

The ''Teach'' key on the 30 mm diameter XX930 range of ultrasonic sensors is expected to have an operational life of around 1,000,000 operations, assuming an operating force of one Newton.
Was this helpful?
What can we do to improve the information ?