Technical FAQs

Ask a Question

What force is required to activate the lever of an XF9Fxx?

The actuation force for the XF9Fxx lever is 1.5 daN (15 Newton or 1.53 Kgf).

There are documents in existence which indicates a "minimum actuation speed of 2.5metres/sec". This is incorrect, it is an administrative/printing error which has been replicated in a number of documents but internal technical document Vantive 1133853 confirms this to be an error and should read "maximum actuation speed 2.5metres/sec"
Was this helpful?
What can we do to improve the information ?