Technical FAQs

Ask a Question

What is the reference number of the orange coloured two-hand control unit?

The XY2SB**  two-hand control units, are supplied painted, orange RAL 2008.
See attachments
 XY2SB Two hand control colour
Note:  The colour of the control unit is not a requirement of the standard (EN574).
Was this helpful?
What can we do to improve the information ?