Technical FAQs

Ask a Question

Can I run a Vijeo Look V2.5 application in a Vijeo Look V2.6 Runtime?

It is possible to run a BuildTime V2.5 application in Vijeo Look V2.6 Runtime. When transferring the application to the Runtime module, the module will request the client to accept the update of the application to version V2.6.
Was this helpful?
What can we do to improve the information ?