Technical FAQs

Ask a Question

How can I modify the configuration of the FTB1IB16EP1 programmable modules?

To modify the configuration of FTB1IB16EP1 modules from 8 inputs/8 diag to 16 inputs, write the value 1 in the 2nd output word. To return to 8 inputs/8 diag, you need to write 0 in this word again.
Was this helpful?
What can we do to improve the information ?