Technical FAQs

Ask a Question

Which operating systems are supported by Modbus Plus MBX Driver V7.0

Modbus Plus MBX Driver V7.0  is validated for use on Windows Vista, XP Professional, 2000, Server 2008 and Server 2003.
Was this helpful?
What can we do to improve the information ?