Technical FAQs

Ask a Question

Must I use the CMD Tool software proposed by Phoenix Contact to configure the M1 PLC Interbus network?

To configure devices on the Interbus IOBUS network for M1 PLCs it is preferable to use Modsoft 2.61 or Concept 2.2 SR2.

Caution: Access to the M1 via CMD Tool does not display diagnostic information.
Was this helpful?
What can we do to improve the information ?