Technical FAQs

Ask a Question

Can I use the MBKT connectors and the T junctions 990NAD23000 on the same Modbus Plus network ?

It is possible to use MBKT connectors and 990NAD23000 T junctions on the same Modbus Plus network. The only restriction is that the continuity of the data signals is maintained. This simply means that pin 1 of the MBKT connectors  (white wire)  must be connected to the white terminals of the T junctions and that pin 3 of the MBKT connectors (black wire) must be connected to the black terminals of the T junctions.
Was this helpful?
What can we do to improve the information ?