Technical FAQs

Ask a Question

How much space do I need around a GenieEvo switchboard

GenieEvo should be installed in a clean, dry, well ventilated substation whose climatic conditions are controlled to stay within those specified in IEC 62271-200 clause 2.1.1. GenieEvo has been tested to IEC 62271-200 for internal arc classification AF and requires the following minimum dimensions: -
  • From back of switchboard to rear wall - 800mm
  • From end of switchboard to side wall - 500mm
  • From floor to ceiling - 3000mm
A minimum operating space at front of switchboard - 1000mm

If the dimensions are smaller than those detailed please contact Schneider Electric
Was this helpful?
What can we do to improve the information ?