Technical FAQs

Ask a Question

What is the part number for Spare barrel lock for Powerpact 4 MG6C6?

Powerpact 4,  MG6C6 comes with lock as standard however spare locks are available.
Spare Barrel lock & keys  = Part No :MGPP4S007
Spare keys ( pair)= Part No : MGK33 = spare keys only pair
The above are also used on the MG25C2, MG25C4,MG25C2M, MG25C4M, MG2C5,MG2C7, MG2C9, MG2C13. Mg6C6,MG6C12,MG6C18, MG8C6, MG8C12 and MG8C18
Was this helpful?
What can we do to improve the information ?