Technical FAQs

Ask a Question

Can you provide longer screws as my back box is deeper than the screws provided?

M3.5 x 50mm screws are available  and the part number is USCREW50** (Replace ** with the suffix code to denote finish required)

SS  - Stainless steel
PW - Painted White
PN - Pearl Nickel
PB - Polished Brass-
PC - Polished Chrome
BN - Black Nickel

M3.5 x 75 mm screws are also available in our Installation Materials Range Part number 3746192

M3.5 x 35 extension studs are also available in our Installation Materials Part number 3746758
Was this helpful?
What can we do to improve the information ?