Technical FAQs

Ask a Question

I would like a BT Secondary and RJ45 cat5 on a single plate?

This combination can be acheived by using Euro modules GUE7062W (BT sec) and GUE7071W (RJ45) on a 2 module Euro modular plate.

or

GUGTELS***  and GUGRJ45*** (Replace *** with the suffix code to denote finish/interior colour required) and a 2 module Ultimate or Exclusive Euro  plate
Was this helpful?
What can we do to improve the information ?