Technical FAQs

Ask a Question

Do the Ultimate Low profile range metal plate finishes match those of the Ultimate Flat Plate range?

 
Low profile is available with polished chrome or brushed chrome finishes only. Note that the Brushed Chrome finish is not the same as the Stainless Steel finish within the flat plate and screwless ranges. This also means that there is currently not a brushed chrome rocker cap on the modules
Was this helpful?
What can we do to improve the information ?