Technical FAQs

Ask a Question

Can I purchase additional screw capped covers for the Ultimate product range if the ones supplied are lost?

Remember the Ultimate range is supplied with two sets of screw caps. Therefore it is recommended one set is left clipped to the back of the front moulding ready for refurbishment in the coming years. The screw cap cover part number is GUMSCO and are in packs of 100

Was this helpful?
What can we do to improve the information ?