Technical FAQs

Ask a Question

I have an Infrascan PIR and the load stays off for no apparent reason?

Perform the following checks:

  • Check for an ‘override off’ switch in the ‘off’ position.
  • Check that the light level adjustment is not set darker than what can be achieved.
  • Check that the lamp has not blown.
  • Check that the circuit breaker or RCD has not tripped
Was this helpful?
What can we do to improve the information ?