Technical FAQs

Ask a Question

I have an Infrascan PIR and the load stays on or comes on for no apparent reason?

Perform the following checks:

  • Check for an ‘override on’ switch in the ‘on’ position.
  • Check that the timer adjustment has not been set for a longer period than expected.
  • Check that there are no plants or branches moving in the wind or animals within the detection area.
  • Check that the Infrascan is mounted firmly.
  • Check that the installation is correctly wired
Was this helpful?
What can we do to improve the information ?