Technical FAQs

Ask a Question

What are the chemical resistant properties of the 56 Series range

It is well documented that Clipsal’s standard grey products are ideal for most applications.
For those environments where harsh chemicals are used that require special chemical resistant properties, Clipsal offers the Chemical Resistant Orange (RO) range

This range has been developed by leading plastic material manufacturers and offers greater resistance to chemical attack than common plastic materials with minimal reduction in impact strength.
To make selection of the correct product easy, we provide the following information  as a guide.

NOTE. This table should be used as a guide only. Any end user should test to evaluate the suitability of any chemical with any plastic




Was this helpful?
What can we do to improve the information ?