Technical FAQs

Ask a Question

How do I replace a lost or damaged Smart Wireless Lighting Controller?

If a Controller is damaged or lost, obtain a replacement and find the record made of the switch settings on the old Controller then duplicate these exactly on the new Controller. Since all the channel and scene settings are stored in the Receivers, no reprogramming is necessary.

In 2011 Smart was replaced by Sphere lighting control and the two systems are not interoperable. Smart products will be available for faulty replacements. Please contact the Technical Helpline on 0870 608 8 608 for details
Was this helpful?
What can we do to improve the information ?