Technical FAQs

Ask a Question

How will I know when my batteries need changing on my Smart Wireless Lighting Controllers?

The right hand LED on the Controller will flash every time one of the buttons is pressed. To replace the batteries please follow the instructions below

Handheld Controller
To change the batteries in the Handheld Controller press in the button located at the base of the back cover and remove it, exposing the battery holder.
Slide out the holder and remove the discharged batteries by inverting the holder. Replace the 2 x CR2032 button cell batteries fitting them both
with the positive (+) symbol facing up. Do not use pliers or tweezers to hold the batteries as this could cause a malfunction. Slide the battery holder into the Controller
casing. Reassemble the Handheld Controller.

Was this helpful?
What can we do to improve the information ?