Technical FAQs

Ask a Question

What is the recommended number of Low Voltage transformers that can be connected to an individual Electronic dimmer switch?

It is recommended that a maximum number of 5 Low Voltage transformers should only be connected to an individual Electronic dimmer switch. The rating should not exceed the rating of the dimmer switch or plate rating if more than on dimmer is included on a plate
Was this helpful?
What can we do to improve the information ?