Technical FAQs

Ask a Question

What Type of mains voltage Tungsten Halogen lamps can I use with Electronic dimmers?

When using mains voltage Tungsten Halogen lamps (GU10), it is essential that these types of lamps incorporate internal fuses and are from quality lamp manufacturers. The use of inferior low quality lamps without internal fuses is not recommended and will invalidate any guarantee or warranty supplied with the dimmer switch

Using dimming electronic transformers and low voltage halogen lamps eliminates potential end of life issues with mains halogen and incandescent lamps.
Was this helpful?
What can we do to improve the information ?