Technical FAQs

Ask a Question

Can the cassette used to connect the circuit breakers to the Powerpact 4 panelboards be ordered separately.

No, the cassette is factory fitted to the MGP... range of circuit breakers.

If you require a circuit breaker that's not available in the standard MGP... range, please contact technical support on 0870 608 8 608 for further information.
Was this helpful?
What can we do to improve the information ?