Technical FAQs

Ask a Question

The single pole circuit breakers used in the Powerpact 4 panelboards used to be marked R, Y or B. How are they marked now?

The single pole circuit breakers used in the Powerpact 4 panelboards used to be marked R, Y or B. They are now marked L1, L2 or L3 respectively..
Was this helpful?
What can we do to improve the information ?